CIMPLICITY REST API Web Service
CIMPLICITY REST API Web Service / ProjectData Json Schema
ProjectData Json Schema
Description
Information about the CIMPLICITY project
Overview
ProjectData
Information about the CIMPLICITY project
projectId : string
the projectId that was searched for
name : string
the name of the project file without the .gef
description : string
the configured description of the project
isReadOnly : boolean
is the project read-only?
readOnlyReason : string
a message indicating why the project is read-only
Properties
NameDescriptionData Type
the projectId that was searched forstring
the name of the project file without the .gefstring
the configured description of the projectstring
is the project read-only?boolean
a message indicating why the project is read-onlystring
See Also